DRV.NAME

Description

This parameter is used to set the name of the drive. The assigned name is one way to identify the drive on a network such as a TCP/IP network on which multiple drives reside. The name is restricted as follows:

  • Only use ASCII characters
  • Max length of 10 characters
  • No spaces in name

Examples

Usage

Issuing DRV.NAME from the terminal with no value will return the name of the drive.

Code

-->DRV.NAME My_AKD2G
-->DRV.NAME
My_AKD2G
-->

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

N/A

Default Value

no_name

Data Type

String

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.